This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
Yes, body diodes can be deliberately used.
Diodes will be formed between drain and source, due to the structure of the MOSFETs. This is called body diodes or parasitic diodes. The N-channel MOSFET cross-section (Fig. 1.1) and equivalent circuit (Fig. 1.2) is as shown below. (Body diode is shown in red.)
The body diode can be used to recirculate the motor current when operating the motor. For example, the high side MOSFET of OUT1 will be turned ON (t1) and OFF (t2) during asynchronous PWM control as shown in Fig. 2. During OFF (t2) period, the recirculating current will flow through the body diode of low side MOSFET of OUT1.
Note that during synchronous PWM control, the low side MOSFET will turn ON during recirculation as shown in Fig. 3, t3. Generally, using MOSFET instead of body diode for recirculation is more efficient and can reduce heat generation.
Also, dead time (t2, t4) is implemented to avoid shoot-through current during synchronous PWM control, in which body diodes will be used for recirculation.
In most cases when setting the motor from rotation state to coast, all MOSFETs will be turned OFF. During which, the body diodes will be used to recirculate the motor current as shown in Fig. 4.
The following documents also contain related information.