Model-Based Development (MBD) Technology to Resolve EMC Issues at the Early Design Stage

We have established a model-based development (MBD) technology that enables highly accurate prediction of EMI and EMS characteristics at the circuit design stage for automotive ICs.
This technology allows EMC-related issues—which have traditionally been identified in the later stages of development—to be resolved at an early design phase, significantly reducing the risk of redesign.

Market Background Driving the Need for MBD

The automotive industry is undergoing a major transformation. With ECU consolidation driven by zonal architectures, the risk of malfunction due to EMI affecting other ECUs, as well as EMS-induced failures within IC circuits, is increasing.
To ensure safety in autonomous driving systems, automotive semiconductor devices such as communication ICs are required to have strong EMC robustness. As a result, resistance to malfunction caused by EMI/EMS is becoming more critical than ever.
At the same time, there is an increasing demand for shorter development cycles, making simulation-based verification essential.
Against this backdrop, we are focusing on the development and provision of highly accurate models for automotive semiconductor devices, as well as the enhancement of MBD-based verification technologies.
In addition to electrical circuit simulation, these technologies support:

  • Electro-mechanical coupled analysis incorporating actuator models
  • Transient thermal analysis
  • EMI/EMS analysis

EMI (Electromagnetic Interference) Simulation Technology

For EMI and EMS analysis, we developed a highly accurate model using an automotive communication IC (TB9032FNG).
During IC development, a trade-off arises: smoothing the driver output waveform to reduce EMI makes it difficult to meet AC characteristics defined by communication standards (ISO 20794).
By utilizing high-accuracy simulation, we optimized this trade-off.
Specifically, the following techniques were applied:

  • Slew rate control for the rising and falling edges of the BUS waveform
  • Edge rounding control (Figure 1. (1)–(3))

By smoothing sharp transitions in the BUS waveform, an improvement of 5–15dBµV in EMI characteristics (150Ω method) was achieved.
In addition, rounding control suppresses switching noise caused by undershoot (ground bounce) during transitions to the dominant (Low) state.
The impact of these measures on EMI characteristics can be evaluated at the circuit design stage through simulation. As shown in Figure 2 (Green line), noise spectrum reduction can be confirmed by BUS waveform control.

Figure 1.  Measured CXPI bus waveform with edge rounding control applied (Figure 1. (1)–(3): Examples of waveform shaping control)
Figure 1. Measured CXPI bus waveform with edge rounding control applied (Figure 1. (1)–(3): Examples of waveform shaping control)

EMI (150Ω method) measurements were also conducted using actual TB9032FNG samples developed through this validation process.
Figure 2 compares measurement results with simulation results, demonstrating strong agreement and confirming the high predictive accuracy of the model.
This enables quantitative prediction of EMI reduction effects and allows optimization of noise mitigation at the design stage.

Figure 2. Comparison of measured and simulated EMI results (150Ω method) (Device: TB9032FNG)
Figure 2. Comparison of measured and simulated EMI results (150Ω method) (Device: TB9032FNG)
Figure 3. Comparison of measured and simulated EMS results (DPI method) (Device: TB9032FNG)
Figure 3. Comparison of measured and simulated EMS results (DPI method) (Device: TB9032FNG)

EMS (Electromagnetic Susceptibility) Simulation Technology

Simulation at the circuit design stage is also effective for EMS.
When external noise such as that used in the DPI (Direct Power Injection) method is applied during semiconductor evaluation, it can cause malfunction of internal semiconductor devices and circuits.
To prevent such issues, it is essential to verify IC robustness at the circuit design stage.
Verification is performed by analyzing:

  • Sensitivity of parasitic transistors
  •  Spatial relationships between devices

and confirming the absence of issues through simulation.
As shown in Figure 3, a strong correlation between simulation and measurement results has also been confirmed for the DPI method.

Summary

Through the TB9032FNG case study, we confirmed strong correlation between simulation and measurement results for both EMI and EMS using MBD.
By utilizing highly accurate IC models, simulation can be extended to include surrounding passive components and printed circuit boards, enabling system-level verification.
In conventional automotive system development, EMC evaluation has typically been conducted in the later stages—after final components are available—often leading to redesign when issues are discovered.
Our approach significantly reduces this risk and enables shorter development cycles.
Going forward, we will continue to contribute to both enhanced reliability and reduced development time for automotive systems by providing semiconductor device models aligned with industry needs, and by delivering solutions suitable for next-generation architectures.

Model-Based Development (MBD) initiatives for automotive semiconductor products
To realize MBD, we provide automotive semiconductor models that are compatible with customers' design environments. We will introduce various SPICE models, thermal analysis, and an overview of our efforts in noise verification.
MBD / SPICE models / Thermal analysis models / Automotive semiconductors / EMC / MATLAB® / Simulink®

聯繫我們

技術方面問題

聯絡我們

聯絡我們

常見問題

常見問答

* Company names, product names, and service names may be trademarks of their respective companies.

開啟新視窗