What is Break Before Make (TBBM)?

This is a bus switch with an SPDT configuration, which specifies that two switches cannot be turned on at the same time when switching.

TBBM is an abbreviation for Time Break Before Make, and it refers to the regulation of the time that two switches must be turned off to prevent both switches from being turned on at the same time.
By setting this regulation, it is possible to prevent two signals from being shorted.

※In general, turning on a switch is called Make and turning it off is called Break.

Table-1 TBBM specification of TC7PCI3212MT

A brief explanation is given using the data sheet of the TDS5C212MX (2 differential channel 1-2 multiplexer/demultiplexer). Table 1 shows the TBBM specified in the AC characteristics. At the supply voltage (VCC = 1.65 to 3.6V), a minimum of (55ns) and a maximum of (400ns) are specified. In other words, when switching between the two switches, it is designed so that both switches are always turned off for a period between 55ns and 400ns.

Please refer to Fig. 1 for the method of measuring TBBM. At the supply voltage (VCC = 1.65 to 3.6V), the (Bn+/Bn-) and (Cn+/Cn-) terminals are fixed at 1.2V, and the SEL terminal is switched between High and Low to switch between the two switches. If there is a period during which both switches are turned off at the same time as the switching timing, the An+/An- terminals go Low (VOL). The period during which the two switches are turned off at the same time is measured.

Table-1 TBBM specification of TDS5C212MX

Fig. 1 Measure method of TBBM for TDS5C212MX
Fig. 1 Measure method of TBBM for TDS5C212MX

This specification is also specified for load switches, etc.

Related Links

The following documents also contain related information.

FAQs

Product Lists

Application Notes

開啟新視窗