This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
The same differential pair combination can also transmit signals with reversed positive and negative pairs, regardless of the product's terminal name.
For example, Fig. 1 shows how to connect a 2:1 Mux (multiplexer) /1:2 De-Mux (demultiplexer) type bus switch.
With this type of bus switch, as shown in the figure below, the destination of the An± terminal can be selected from either the Bn± or Cn± terminal, enabling bidirectional communication.
When terminals An± and Bn± are connected, An+ and Bn+ and An- and Bn- are internally connected. Therefore, even if a differential signal whose positive and negative are opposite to the terminal name is input, the path inside the switch will be the same as in normal use as shown in Fig. 1. The positive and negative of the signals output from each terminal are opposite to the terminal name.
The following documents also contain related information.