This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
Do not leave unused input pins of CMOS logic IC floating and connect them to VCC or GND as shown in Fig. 1. In the floating state, unexpected output or oscillation may occur due to disturbance noise, etc.
The bus pins (I/O pins) of 74xxx245 and other bidirectional bus buffers are floating when /G pin is set to High. When /G pin is High, connect the bus/output pin to VCC or GND with a resistor as shown in Fig. 2.
In addition, do not apply an external signal when the bus pin is in output mode.
Products with a bus-hold function (such as 74VCXH) do not require an external pull-up or pull-down resistor.
Please refer to here for bus hold.
FAQ: What is bushold of the general-purpose logic ICs?
The following documents also contain related information.