This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
The NOT circuit is also called the logic negation circuit.
When 1 is input to A, the output becomes 0, when 0 is input to A, the output becomes 1.
In this way, the input signal inverted and output.
The schematic can be expressed by the MIL symbol as shown in the right figure.
A NAND circuit is configured by combining the NOT circuit with the AND circuit.
A NOR circuit is configured by combining the NOT circuit with the OR circuit.