This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
型號需要超過三個文字以上 Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
型號需要超過三個文字以上
The “R” and “S” of the RS flip-flop circuit are abbreviations for "Reset" and "Set" respectively.
In order to have the memory function for flip-flop, it is necessary to retain the output state by giving feedback on the output state to the input.
When both R and S are “0”, if Q is “1”, it retains “1”, and if it is “0”, it retains “0”.
The state where Q stores "1" is called the set state, and the state where it stores "0" is called the reset state.
The output terminals have Q and Q, but the relation between Q and Q is always reversed.
In the operating conditions of the truth table, it has the condition which is prohibited, but if it is used by this condition, the next output cannot be determined.
Below in the right figure is a time chart of the RS flip-flop circuit. When the input signal “1” is set to S, the output terminal Q is set.
After that, if both S and R continue to be “0”, Q maintains the set state.
Next, if R becomes “1”, it is reset and the reset state is retained until the input signal is set to S again.
In this way, the RS flip-flop circuit has the property of storing a momentary signal as data.